Space and Equipment Report - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

To view the Spaces and Equipment report, open the generated .csv file in Microsoft Excel. We recommend you create a pivot table in Excel to view the report.

The Spaces and Equipment report displays the following information in a report:
  • Equipment: Each piece of equipment is displayed individually by row for a Space.

    Note: A Space can have multiple pieces of equipment associated with it.
  • Space Levels: Space levels for the site are captured in unique columns within the report.

    Note: There is a limit of ten nested levels under any given space object.
  • Equipment Name: Equipment Names refer to the specific identification name of the device or engine.

  • Equipment Fully Qualified Reference (FQR): Equipment FQRs refer to location of the piece of equipment in the Equipment Tab.