Object Count by Device Report - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

To view the Object Count by Device report, open the generated CSV file in Microsoft Excel.

The Object Count by Device report displays the following information in a report:

  • Archive: name of the archive.
  • Device Name: name assigned to the supervisory device (engine) in the archive.
  • Device Release: Metasys system release of the supervisory device in the archive.
  • Object Count: total number of objects defined under the supervisory device.
  • Firmware Version: firmware version of the supervisory device.
  • Model Name: name assigned to the device (unknown if no model name is defined).
Figure 1. Object Count by Device Report