Re-index - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

Menu Selection: Tools > Database > Re-index

Using the Re-index feature improves SCT performance against large archive databases. The Re-index feature removes fragmentation from the archive database. A clock appears during the re-indexing process.

Note: Re-index works against any size archive and is especially recommended for sites containing more than 100 NxEs.