Create Backup - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

Menu Selection: Tools > Database > Create Backup

Creates a backup file for the active archive database, including network engine self-signed and trusted certificates, if in use. If needed, the archive database can be restored using the Tools > Database > Restore Backup menu option. See the Restore Archive.

The backup file is always named <archive>.backup, where <archive> is the name of the open archive visible at the top of the SCT navigation tree. Do not rename the backup file (renaming a backup file causes a subsequent restore to fail). To save different versions, copy the backup file to different subdirectories.

The default path is C:\ProgramData\Johnson Controls\MetasysIII\DatabaseFiles.