System Preferences - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020

System preferences apply to all users who log in to the site or device. System preferences affect the performance and operation of the system and require authorization to configure. A change to the audible alarm notification is an example of a system preference. Only the users defined in the Users Authorized to Edit System Preferences section are authorized to configure system preferences.

To synchronize system preferences within a site or to reuse the system preferences on another site, refer to the Configuring and Maintaining Preferences appendix of the ADS/ADX Commissioning Guide (LIT-1201645) , ODS Commissioning Guide (LIT-12011944) , or the NAE Commissioning Guide (LIT-1201519).