Metasys Preferences Dialog Box - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

The Metasys Preferences dialog box is accessed through the Tools menu (Configure Preferences) and allows you to configure system and user preferences. Users authorized to edit system preferences can edit all preference fields using the Metasys Preferences dialog box. See Users Authorized to Edit System Preferences. Unauthorized users can edit only user preferences.

Some of the preferences defined in the Metasys Preferences dialog box also apply to the Metasys UI. The following table calls out the tabs with such preferences. See the specific tab section for details.

Click the tab name in the table for a description of the Metasys Preferences tabs. For more information on the modes of operation, see Metasys Modes. The Authorization Required column means you must be authorized to edit some or all of the preferences located on that tab.

Table 1. Metasys Preferences Dialog Box Tabs for SCT, Metasys UI, and SMP
Tab

SCT

Applies to Metasys UI Applies to SMP UI Authorization Required

Information Tab

X

 

X

 

Graphic Settings Tab

X

X

X

X

Display Settings Tab

X

X

X

X

Applications Tab

X

 

X