Preferences - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

The Metasys system provides customized preferences for the user interface. The preferences allow you to configure how the user interface behaves, including its sounds and colors, startup views, alarm priorities, and the ability to add links to external applications that can be accessed from within the UI.

Some of the preferences defined in the Metasys Preferences dialog box also apply to the Metasys UI. The Metasys Preferences Dialog Box section calls out such preferences.