Download Certificate - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

Use the Download Certificate option to download server certificates independently from other actions. This method is much faster than if you were to download the full database with the Download To Device option in the Manage Archive wizard.

When you download certificates to a site device, SCT determines the correct set of certificates required by that device for successful site configuration. If any certificates are missing, SCT includes the set of certificates that it recognizes during the download, but the missing certificates need to be imported before trusted connections can be established. Also, no certificates are downloaded if the server certificate and private key for that device are not present in the SCT archive.

Note: From Metasys Release 10.1, network engines require additional security certificates to be stored locally on the devices. When you download certificates, all of the certificates stored in the SCT archive are transferred to a network engine.