Importing a Portion of an Archive Database from a File - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020

About this task

Note: For more information, see Import Item.

The data file to be imported must be in the following directory:

C:\ProgramData\Johnson Controls\MetasysIII\DatabaseFiles

To import part of an archive database from a file:

Procedure

  1. Open an Archive database.
  2. On the Item menu, select Import Item. The Import wizard appears.
    Figure 1. Import wizard

  3. Select the file you want to import and click Import.

    Importing a file discards all change status indicators (the little green arrows in the navigation tree) from your database. Importing a Site Director into a database with existing User Views is not supported and may cause loss of User View data.

    When the import is complete, the new item appears in your navigation tree.