Deleting an Archive Database - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

About this task

Only one archive can be deleted at a time. An open archive can be deleted.

To delete an archive database:

Procedure

  1. On the Item menu, select Delete Archive.
    The Delete Archive wizard opens.
  2. Select the archive to delete and click Delete.
  3. Confirm the deletion.