Copying an Archive Database - Metasys - LIT-12011964 - MS-SCTRMOT-0 - MS-SCTSWO-0 - MS-SCTSWO-6 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020

About this task

The Archive copy must have a unique name. By default, the new archive has the same name as the one you are copying with a number appended to the name.

To copy an archive database:

Procedure

  1. With an archive database open, select Create Archive Copy from the Item menu. The Copy Archive wizard appears.
  2. Select the archive to copy from the list.
  3. Type a name for the new Archive database copy in the right pane of the wizard.
  4. Click Copy.
  5. Click Yes when prompted to close the current database. The new Archive copy opens.