Deleting Trends from the Trend Study - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

Procedure

  1. View the Trend Study.
  2. Click the Definition View button.
  3. Click the Edit button.
  4. Select a trend in the Trend Item table.
  5. Click the Remove icon. The Remove confirmation dialog box appears asking if you want to remove the trend item. Click Yes.
  6. Click Save.