Configuring the Metasys Server / ODS as the Destination for Trend Data - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

About this task

Notes:
  • You can define only one repository as the default destination.
  • If you need to provide long-term storage for trend samples from an Engine, follow these steps to configure the Trend Repository of a Metasys server as the Default Destination.

To configure the a Metasys server Trend Repository as the Default Destination for trend samples from an Engine:

Procedure

  1. Select the Engine device in the navigation tree.
  2. View the Engine. See Displaying Information About an Item for more information on how to display an item.
  3. Select the Focus tab and click the Advanced radio button to display additional item information.
  4. Select Edit.
  5. Edit the Metasys server Repository and the Metasys server Delivery Time. (The Engine Device Object attributes table contains Default Value and Values/Options/Range information for the attributes.)
  6. Click Save.
    Note: If you want to define the a Metasys server attributes for the entire site instead of at the individual Engine level, select the Site in the navigation tree and edit the Metasys server Repository and the Metasys server Delivery Time. (The Site Object attributes table contains Default Value and Values/Options/Range information for the attributes.)