Chart Legend - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020

The Chart Legend appears below the graphical charting area. The Chart Legend displays the list of trend items for the Trend Study in a table, and includes information about each item.

Table 1. Legend

Button/Field

Name

Description

Select All

Selects the maximum number of trend items for display in the chart.

Remove All Selections

Deselects all trend items in the chart Legend.

Show

Indicates if the trend item appears in the Chart. When checked, the data appears on the chart and in the table. When unchecked, the data does not appear in the chart or table.

Historical Trend Icon

Indicates the trend was selected from the Metasys server Historical Database folder.

Marker

Indicates the appearance of the marker style and color for the trend item on the Chart.

Color Palette

Displays the Select a Color dialog box. Allows you to change the color used to chart the trend data.

 

Name

Displays the trend item name based on the Name attribute.

 

Reference

Displays the trend item’s full reference.