Accessible through the navigation tree, Trend Studies display trend sample data from trends in Engine trend buffers and/or Metasys server repositories. A Metasys server on the site is not required to retrieve trend data from the Engine.
When you create a Trend Study, you use the Trend Study wizard to choose the sources for the trends and the display properties.
An Audit Trail message is created whenever you create, delete, or edit a Trend Study. Trend Studies, graphics, and folders are the only items you can create under a Metasys server on the navigation tree.
The main advantages to using Trend Studies are that you can:
-
view multiple trends at once (from both Engine and Metasys server )
-
view Metasys server historical trend data
-
configure the Study Range with flexible parameters