Trend Study - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

Menu Selection: Insert > Trend Study

Inserts a trend study into the site.

Tip: With the Trend Study tab selected on the Configure Screen, select the plus icon to add trend items, or click the minus icon to remove trend items.
Tip: Select the Configuration tab on the Configure screen for further configuration.

See one of the following sections for more information: