Operating System - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

Engines use a Microsoft Windows Embedded or Linux operating system (specific operating system depends on the model), which is shipped preinstalled on the Engine or can be updated after the engine is installed. In general, the operating system cannot be modified by adding or deleting programs or drivers, although provisions are made to install factory-authorized patches and upgrades.