Flash Memory - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

A type of nonvolatile memory within the Engine device. The Engine stores the operating system, software, and archive within this memory. This memory is not used during normal operation of the Engine device, except when a new graphic is added and the new image is uploaded and stored. The flash memory is mostly used during shutdown and system restart.