Database - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

The database is the collection of objects and their parameters as defined by the user. Each database is unique to the job. A database can be created or edited (with appropriate user authority) either online using the Site Management Portal UI, or offline using SCT. SCT can also be used to download a database or upload and create a backup copy of the database.