Archive - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

A copy of the database, called the archive, is kept in each Engine’s flash memory. This happens automatically once a day or on operator command. Following restoration of power loss to an Engine, the archive is copied into main memory to restore normal operation.