Reusing an Existing Summary Definition for Different Key Data - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

About this task

Use this procedure if the key data is the only thing that is different between two different views (for example, establishing the key data for individual Air Handlers with their associated VAV boxes).

Procedure

  1. Export an existing Summary Definition. See the Exporting a Summary Definition section.
  2. Rename the Summary Definition.
  3. Import the renamed Summary Definition. See the Importing a Summary Definition section.
  4. Make the necessary Object Name and Key Data changes. See the Defining Key Data section.
  5. Add the Summary Definition to the desired user view. See the Defining User Views with Summary Definitions section.