Importing a Summary Definition - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

Procedure

  1. In the All Items tree, right-click the Summary Definitions folder and then click Import Definition.
  2. Browse to the location on the computer where the Summary Definitions are stored.
    Note: You can download a set of pre-built Summary Definitions from the Johnson Controls License Portal and save these files to your computer. You also can import previously exported Summary Definitions. See the Exporting a Summary Definition section.
  3. Select one or more Summary Definitions to import.
  4. Click Import. The Notice dialog box appears, indicating the results of the import after all imports complete.
    Figure 1. Notice Dialog Box

  5. Click OK. The imported Summary Definitions appear in the Summary Definitions folder in the All Items tree.