Defining User Views with Summary Definitions - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2
Metasys SCT: System Configuration Tool Help
- Product
- Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
- Document type
- User Guide
- Document number
- LIT-12011964
- Version
- 13.2
- Revision date
- 21/01/2020
Procedure
-
Create a user view or edit an existing one (for example, an HVAC user view).
-
Add a folder to the user view to hold the Summary Definitions. For example, add a Summary Definitions folder, or a folder named according to function (such as VAV Boxes - VMA1400s, Key Point Information, Engines, or MSTP Trunk Diagnostics).
-
Drag the definitions from the Summary Definitions folder in the All Items tree
to the folder you created in the user view (or use the user view editor’s add
reference option).
-
Drag the items to reference (for example, supervisory devices or points) from
the All Items tree or from the global search results table to the folder in the
user view (or use the user view editor’s add reference option).
-
Save the user view.