SCT Summary Definition Attributes - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

This object contains attributes common to many Metasys system objects. These common attributes are described in the Common Attributes section. For information on the Tailored Summary Viewer feature, see Tailored Summary Viewer.

Click the attribute name in the table for a description of the attribute.

Note: In the notes column, attributes marked with the letter C are configurable, attributes marked with the letter N do not require a value, and attributes marked with the letter W are writable.
Table 1. SCT Summary Definition Object Attributes - Focus/Configuration Tab

Attribute Name

Data Type

Notes

Initial Value

Values/Options/Range

Name

Text

CW

 

Maximum Length of 400 characters

Description

Text

CN

 

Maximum Length of 40 characters prior to Release 8.0 and 64 characters at Release 8.0 and later.

Authorization Category

One type from a set

C

General

HVAC, Fire, Security, Services, Administrative, General Lighting, Refrigeration, Critical Environment, Air Quality, Power, Energy, System Custom 1-150

Table 2. SCT Summary Definition - Summary Definition Tab

Attribute Name

Data Type

Notes

Initial Value

Values/Options/Range

Column Heading

List of Structures

C

 

Column Heading, Child Item, Attribute

Row Headings Column Text

Text

CN

 

Label

Maximum Length of 50 characters

SCT Summary Definition Attribute Details

Column Definition defines the columns displayed in the Tailored Summary Viewer in the SCT. You can define up to seven columns (list of structures). Each structure contains the following information:
  • Column Heading - Defines the name of the column header.
  • Child Item - Indicates item for which the column data is retrieved based on its name attribute, which must match a user-specified pattern (such as ZN-* or ZN-T, or Zone-T). To display an attribute of the row item, leave this field blank. Otherwise, specify the name of the child item to display.
  • Attribute - Defines the attribute information for the column. The attributes are grouped into categories for easy selection. Select a category in the Attribute Filter section of the Select Column Attribute dialog, and then select the desired attribute from the list.