Program Object - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020

The Program object (previously the Control System object) stores information needed for the user-defined control strategies created (graphically) with the Logic Connector Tool (LCT). The Control System object application now includes BACnet command object functionality and appears as the Program object in the Metasys software. The Program object attributes allow manipulation of the LCT application.

For general information on Metasys system objects, see Common Object Attributes.