Saving a Control System - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

To save a control system, click Save on the Toolbar. The LCT scans for logic errors.

Notes:

  • The logic check done with the Save command is not the same as the Logic Checker run from the toolbar.
  • If inputs are missing, an error message appears asking if you want to continue with the save. Click No to return to the logic. Click Yes to save anyway. We do not recommend saving with errors.