Editing TMR (Timer) Blocks - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

About this task

To edit TMR (Timer) blocks in Edit mode:

Procedure

  1. Double-click a Timer block. The TMR dialog box appears.
  2. Edit the timing functions of the block.
    Table 1. TMR (Timer) Block Configuration

    Field

    Description

    Duration

    Specifies the length of the timer function in seconds. The range is 5–86,400 seconds.

    Setup

    Determines the type of timer you use:

    • Pulse
    • On Delay
    • Off Delay
    • Minimum On
    • Minimum Off

    OK

    Accepts changes.

    Cancel

    Cancels changes.