About this task
To edit System Blocks in Edit mode:
Procedure
- Double-click a System block. The Expose Attributes dialog box appears.
-
Configure the inputs, outputs, and attributes of the subsystem.
Note:
- Select the Add button to add an attribute to configure. To remove attributes from the System, select the check box next to one or more attributes and click the Remove button.
- To view the control system for the System block, drag and drop the control system from the Navigation Tree to the Panel Layout.
- If you click Cancel to disregard
your changes to the System block the changes are not saved, as
expected. However, if you once again edit the same System block, and
an error prompt appears stating
An error occurred. Object does not exist, simply try these steps again. The error does not reoccur with the second attempt.