Editing Math Blocks - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

About this task

To edit Math blocks in Edit mode:

Procedure

  1. Double-click a Math block. The configuration dialog box appears.
  2. Edit the fields and configure the number of inputs based on the selected type of logic.
    Table 1. Math Block Configuration

    Field

    Description

    Input

    The number of inputs depends on the type of Math block you use. You cannot reduce the input count lower than the number of current connections.

    OK

    Accepts changes.

    Cancel

    Cancels changes.