Editing Constant Enum - Metasys - LIT-12011964 - MS-SCTRMOT-0 - MS-SCTSWO-0 - MS-SCTSWO-6 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020
Table 1. Constant Enum

Callout

Description

Enum Category

Set category determined by the user interface (either Two State or Multi State).

Enum Set

Set determined by the category selected in Enum Category.

Enum

Set state determined by the set and set category.

OK

Accepts changes.

Cancel

Cancels changes.