Editing Constant Blocks - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

About this task

To edit Constant Category blocks in Edit mode:

Procedure

  1. Double-click a Constant block. One of two dialog boxes appears depending on the type of constant you select.
    Note: There are no configurable parameters for the Rel. (Release) constant. When you double-click, nothing happens.
  2. Edit fields and configure the constant value (Editing Constant Enum, Editing Constant Float).