Editing Span Blocks - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

About this task

To edit Span blocks in Edit mode:

Procedure

  1. Double-click a Span block. The Span dialog box appears.
  2. Edit the fields to enable or disable clamping.
    Table 1. Span Block Configuration

    Field

    Description

    Clamp High

    Selects whether (True) or not (False) to clamp the Output at the Output High (OH). For more information on clamping, see Span.

    Clamp Low

    Selects whether (True) or not (False) to clamp the Output at the Output Low (OL). For more information on clamping, see Span.

    OK

    Accepts changes.

    Cancel

    Cancels changes.