Editing RL (Rate Limiter) Blocks - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

About this task

To edit RL (Rate Limiter) blocks in Edit mode:

Procedure

  1. Double-click a Rate Limiter block. The RL dialog box appears.
  2. Edit the Rate Limit and Startup Value for the RL block.
    Table 1. RL (Rate Limiter) Block Configuration

    Field

    Description

    Rate Limit

    Specifies the rate per minute to increase/decrease the Output until it matches the Input.

    Startup Value

    Specifies the value the rate limiter block will start at when the engine is restarted and block enable is true.

    OK

    Accepts changes.

    Cancel

    Cancels changes.