Editing Attribute Reference Outputs - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English
Table 1. Attribute Reference Output

Field

Description

Label

Enter a label here for the block.
Note: Do not start labels with a number and then follow it with any of these characters: $ . - ,

Object

Browses to the object to which the reference is linked. Leaving this field blank leaves a placeholder for a future reference. The dragged object’s name appears in this field and the object’s attributes appear in the drop-down list in the attribute field.

Attribute

The attribute to which the reference is linked. When you are configuring an Output reference, the drop-down list contains numeric, writable attributes only.

OK

Accepts changes.

Cancel

Cancels changes.