Editing Attribute Outputs - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Table 1. Attribute Output

Field

Description

Name

Name of the output

Units

The units for the output

Display Precision

Tells the Metasys software what precision to use when formatting data.

This field only appears for floating outputs.
Note: Display Precision is used in the Focus view of data, not the graphical view.

Enum Category

Set category determined by the user interface (either Two State or Multi State).

This field only appears for Enum outputs.

Enum Set

Set determined by the category selected in Enum Category.

This field only appears for Enum outputs.

OK

Accepts changes.

Cancel

Cancels changes.