Editing Attribute Inputs - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020
Table 1. Attribute Input

Field

Description

Name

Name of the input

Units

The units for the output.

This field only appears for floating inputs.

Display Precision

Tells the Metasys software what precision to use when formatting data.

This field only appears for floating inputs.
Note: Display Precision is used in the Focus view of data, not the graphical view.

Enum Category

Set category determined by the user interface (either Two State or Multi State).

This field only appears for Enum inputs.

Enum Set

Set determined by the category selected in Enum Category.

This field only appears for Enum inputs.

Trigger

This is checked if you want the attribute to trigger the control system to execute if its value changes by more than the defined increment.

OK

Accepts changes.

Cancel

Cancels changes.