Re-Routing a Connection - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

Procedure

  1. Make sure the LCT is running in Edit Mode.
  2. Place the cursor over an existing end connection point until the cursor changes into a cursor with lines protruding from the tip.
    Note: You may only move the destination point. To completely change the connection, see Deleting Connections.
  3. Click the connection point. The tool removes the connection.
  4. Click a new connection point. The tool creates the newly routed connection.