Deleting Connections - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020

Procedure

  1. Make sure the LCT is running in Edit Mode.
  2. Select the connection and right-click.
  3. Select Delete from the menu.

Results

OR

  1. Select the connection.
  2. Press the Delete key on the keyboard.