Connecting Blocks - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

Procedure

  1. Make sure the Logic Connector Tool is running in Edit Mode.
  2. Place the cursor over the starting connection point until it changes shape from an arrow to a magic wand and click the point.
  3. Click the ending connection point.

    Notes:

    • If the connection is valid, the cursor is a magic wand. If the connection is not valid, a circle with an X through it appears, and the tool does not connect the points.
    • After you successfully connect two points, the line between them turns blue until you click somewhere else in the workspace.
    • You do not need to click the exact connection point. If you click in the block, the tool automatically creates a connection to/from the nearest block’s connection point. To cancel the connection after clicking the first block, click anywhere in the workspace.
  4. The Priority Connection dialog box appears. Choose a priority from 1–16 (1 is the highest priority).
    Note: To change the priority at a later time, you must delete the connection and reinsert it.