Drag and Drop - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

About this task

To add items to a control system using the drag and drop method:

Procedure

  1. In the Edit Mode of the LCT, left-click and drag an item from the left side of the tool view and drop it in the workspace.

    Notes:

    • If the item is a System block, a configuration wizard appears. Answer the questions to set up the new object/system or create a reference to an object or control system.
    • There is not interaction between the user navigation tree and logic.
  2. Edit the block to match your needs. See Editing Blocks in Edit Mode.