Printing - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

The Logic Connector Tool supports printing of the following paper sizes in either landscape or portrait orientation:

  • Letter (8.5 x 11 in)

  • Folio (8.5 x 13 in)

  • Legal (8.5 x 14 in)

  • Tabloid (11 x 17 in)

  • A1

  • A2

  • A3

  • A4

  • A5

The Logic Connector Tool supports printing of just the existing control system.