System Blocks - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21

System blocks support drag and drop functionality. When you deposit a System block onto the workspace, a configuration wizard guides you through the configuration of the control system. System blocks are useful when you have complex logic because they allow you to nest one control system in another control system. When you create a System block, the Metasys software creates a Program (Control System) Object under the first Program object in the navigation tree.

See Adding Items to Logic.