The following table and figures illustrate the function of the Minimum On timer.
|
Feature |
Description |
|---|---|
|
Activation |
See row below. |
|
Output |
Goes active when there is a low to high Input transition when the timer executes (logic executes every 5 seconds). The Output remains active until the time specified in Duration passes AND the Input returns to inactive. |
|
Reset |
Has no effect on Minimum On timer. |
|
Example |
Keeps a chiller running for a minimum time after startup to stabilize equipment. |
Figure 1. Minimum On Timer Example 1

Figure 2. Minimum On Timer Example 2