Statistical blocks perform statistics on input. The number of inputs to a Statistical logic block depends on the number of inputs supported by the type of statistic. The Logic Connector Tool allows you to add multiple connections to the output of the block.
|
Statistical Type |
Inputs |
|---|---|
|
AVG |
2–8 |
|
MAX |
2–8 |
|
MIN |
2–8 |
See Editing Blocks in Edit Mode for information on editing Statistical blocks.