Control Category - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

Most control logic blocks have three inputs, and you can add multiple connections to the output of the block. The blocks compare input number 1 with input number 2 using the differential (input number 3). The type of control depends on the statistical type. The Sequencer functions differently. See SEQ (Sequencer) for details.

Table 1. Control Blocks

Block

Statistical Type

Inputs

X>Y

greater than

3

X<Y

less than

3

X<=Y

less than or equal

3

X>=Y

greater than or equal

3

<>

not equal

3

=

equal

3

SEQ

Sequencer

See SEQ (Sequencer) for details.

See Editing Blocks in Edit Mode for information on editing Compare blocks.