Constant Category - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020

Constant logic blocks can have multiple connections to the output of the block. Constant logic blocks can be any one of the following:

Table 1. Constant Blocks

Block

Statistical Type

Enum

Enumeration

Float

Float

Rel.

Release

Note: Sends the Release command at a specific priority based on the connection.

See Editing Blocks in Edit Mode for information on editing Constant blocks.