Edit Mode - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020

Access Edit mode by clicking the Edit mode button (see Toolbar). You must be in Edit mode to edit logic or create logic. The LCT opens in View mode.

In Edit mode, you have access to all toolbar items, System blocks, and Logic blocks.

Right-clicking in Edit mode brings up basic choices such as cut, copy, paste, delete, duplicate, hide, label, zoom, and connect, depending on the type of item you select.

Note: Do not start labels with a number and then follow it with any of these characters: $ . - ,

For mouse shortcuts in Edit mode, see Mouse Shortcuts: Edit Mode.