LCT Modes - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English

The Logic Connector Tool runs in either Edit Mode or View Mode.

You can generate logic and make logic changes when you are using Metasys in offline mode (using the SCT) or online mode. (See Metasys Modes.) After generating logic or making any changes to existing logic in offline mode, download the database to the online device to ensure the latest information is used.