General Logic Connector Tool Rules - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
2020-01-21
Language
English
Table 1. General LCT Rules

What Are You Doing?

What Components Are You Using?

These Rules Apply:

Moving, Sizing, Typing

All blocks

  • Left-click to drag and drop blocks
  • Block size is fixed
  • Font size and type are fixed

Connecting

System blocks

Attribute Properties:

  • Read Only
  • Writable
  • Prioritized Write

Connection Type Allowed:

  • Output
  • Input or Output
  • Input, Output, or Both

Connecting

Math, Bool, Statistical, Selector, Control, Psychrometric, Calculation

All inputs should be connected for these Logic blocks. If you attempt to save logic that is missing inputs, an error message displays. You may save anyway or supply inputs where necessary. We do not recommend saving with missing inputs. In the Edit view, blocks with missing inputs have red input points. When the inputs are connected, the connection point turns blue.