Logic Connector Tool (LCT) - Metasys - LIT-12011964 - MS-SCTSWO-6 - MS-SCTSWO-0 - MS-SCTRMOT-0 - Bulb controller - Metasys System Configuration Tool - 13.2

Metasys SCT: System Configuration Tool Help

Product
Building Automation Systems > Building Automation Systems > Metasys System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
13.2
Revision date
21/01/2020

Use the Logic Connector Tool to create the logic within a control system using a graphical presentation. The control logic may include System Blocks and Logic Blocks. The Edit Mode allows you to edit logic, and the View Mode allows viewing and limited commanding capabilities. When running the LCT on the SCT (Metasys system in offline mode), commanding is disabled.

The Logic Connector Tool allows control system viewing and editing through any browser logged in to any online or configuration server with access to a Program (Control System) Object and Metasys system.

Logic runs approximately every 5 seconds. It is important that control applications that require particular timing use internal logic to determine time between executions.

Note: You cannot insert logic on a Metasys server .